Whether PROGDSC TOOL supports bin file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Whether PROGDSC TOOL supports bin file

1,783件の閲覧回数
jacklin_123
Contributor I

i can use .S file  ,but if i use .bin , progdsc tool output message

Error :File not found -or- Unknow file type)

Error: Uable to load object file :.......bin

Or if there are other methods or tools that can be programmed with bin files

0 件の賞賛
返信
1 返信

1,763件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you know that the prodsc.exe tools is  third party tools www.pemicro.com

I suppose that the tools only supports S-Record file, it does not support *.bin file. The S-Record file provides address information, the DSC dose not use united address, it has X: field address and P: field address.

But the *.bin does not have address inf, it can not identify the X: space and P: space.

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信