Whether PROGDSC TOOL supports bin file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Whether PROGDSC TOOL supports bin file

842 次查看
jacklin_123
Contributor I

i can use .S file  ,but if i use .bin , progdsc tool output message

Error :File not found -or- Unknow file type)

Error: Uable to load object file :.......bin

Or if there are other methods or tools that can be programmed with bin files

0 项奖励
回复
1 回复

822 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you know that the prodsc.exe tools is  third party tools www.pemicro.com

I suppose that the tools only supports S-Record file, it does not support *.bin file. The S-Record file provides address information, the DSC dose not use united address, it has X: field address and P: field address.

But the *.bin does not have address inf, it can not identify the X: space and P: space.

Hope it can help you

BR

XiangJun Rong

0 项奖励
回复