Using Freertos instead of NXP SmartDSP OS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using Freertos instead of NXP SmartDSP OS

2,377 次查看
JayCao
Contributor III

Hello,

We are using a Multicore DSP device, and it is using SmartDSP OS.

I would like to ask if I can change it to use Freertos instead.

If possible, please help to share guides to build it.

Thanks and BRs,

0 项奖励
回复
3 回复数

2,359 次查看
JayCao
Contributor III

Hello,

Could you share with us the new MCU product lines replace the StarCore family?

And please include the instruction on how to use Freertos on that instead of NXP OS.

Thank you!

0 项奖励
回复

2,349 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I do not know your application, StarCore is a communication processor. The Starcore family is not recommended in new design, there is not direct replacement, but you can refer to the LA sub-family in Layerscape  family.

https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/layerscape-processors/la...

If you want to understand FreeRtos, I suppose that you order a board from LPC, Kinetis, i.mxrt family, then download SDK package with FreeRtos checked, you can study FreeRtos.

For example, you can order LPC55S69-EVK board and download SDK package.

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...

SDK package:

https://mcuxpresso.nxp.com/en/welcome

 

Hope it can help you

BR

XiangJun Rong

 

0 项奖励
回复

2,366 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that you use StarCore family which supports smartDSP OS, based on the fact that the starcore is not recommended in new design, it is impossible to port the code on FreeRTOS.

Hope it can help you

BR

XiangJun Rong

 

0 项奖励
回复