TEA2017 start up issues

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TEA2017 start up issues

1,542件の閲覧回数
Maxjay
Contributor II

Customer is working on the 150W design (24V/6.25A) now, but currently facing start up when output current is 3A (the pin 15 will be trigger), 2A/4A is normal operation, any idea for this issues? Below is start up waveform Screenshot 2025-03-11 230029.png

0 件の賞賛
返信
2 返答(返信)

819件の閲覧回数
james698goff
Contributor I

Hello,
The issue at 3A startup may be due to SNSCURLLC triggering prematurely—TEA2017 allows this during startup to avoid false OCP. Verify your schematic using the TEA2017 design tool and check if the calculation sheet parameters align with expected startup behavior. Adjusting soft-start or current sense thresholds may help stabilize the 3A condition.

Best Regards,
James Goff

0 件の賞賛
返信

1,513件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi Maxjay

1:代理商的问题我们建议直接提ticket。

这里还是建议客户先用calcualtion sheet核实原理图

2:

在启动的时候是允许SNSCURLLC有动作的是为了防止触发OCP/

0 件の賞賛
返信