TDA5051A DC Power Line Communication

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TDA5051A DC Power Line Communication

4,576件の閲覧回数
roersmat
Contributor I

I have the TDA5051A on a 12VDC power line using the schematic below. 7.372MHz independant oscillator, 115.2kHz carrier frequency. I've tried both 600 and 1200 baud communication.

I can get the transmission to work over short distances (<4ft), but once it gets to about 6-8ft, the communication starts to get lost. See the attached oscilloscope plot showing the degradation over about 4 ft of cable. CH2 is on the output of the transmitter and  CH1 is at the receiver at the other end of the cable. Seems like the carrier signal is getting washed out a bit over the distance of the cable and I'm not sure why that is happening.

Is the amplitude of the carrier signal expected to be so small (~100mV)? I've done simulations of the coupling circuit and it should be much higher (~1.5V). 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

4,456件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi

For your schematic update as below comment then test again:
1:remove C7/C8

2:use 10uF capacitor connect between L1 and TDA5051 PIN10.

3:use 0.1uF capacitor connect between TDA5051 PIN14 and PIN10. 

0 件の賞賛
返信