Switch audio input to SPDIF on a SAF77 chip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Switch audio input to SPDIF on a SAF77 chip

2,129 Views
Nickldio
Contributor I

Hello,

I am trying to switch the audio input on my car radio to SPDIF. The radio has the SAF7730HV chip on it, and I'm struggling to find any documentation on it. However, I found one for the SAF7741. Are they similar enough to work with that instead? I'm looking for the I2C registers to switch the input to SPDIF.

Does anyone have an idea how to achieve this? Is there documentation on NXP's I2C commands for similar chips, assuming they may be the same for mine?

 

Thanks

0 Kudos
Reply
2 Replies

1,613 Views
efefurkan
Contributor I

Hello if you have saf7741 i2c memory map or datasheet different.

Could you share it ?

I am trying some changes on my radio which is using saf7741.

Thank you .

0 Kudos
Reply

2,085 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

It appears that the docs related to SAF7730HV are confidential, pls contact NXP sales or FAE to apply for it.

BR

XiangJun Rong

0 Kudos
Reply