Strange behaviour in DSC´s ADC12

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Strange behaviour in DSC´s ADC12

2,296 Views
cabl
Contributor III

Hi everybody,

 

I´m using DSC56F84789 + CW10.4 + ProcessorExpert to develop a project that samples several channels of the ADC12 (triggered parallel, converter A only, simultaneous). I can see random samples that are close to (or exactly at) 16384, when the sampled signal is a sinusoidal ranged from +5000 to -5000, 50 Hz which a sampling frequency of 6400 Hz. Sampling is perfet appart from these sporadic (once a day, once in a weekend, twice a day...) outliers.

 

Has anyone experienced a similar problem?

 

As I know there´s a bug in PE that generates wrong configuration of ADC, I manually setup up the ADC12 registers like this:

 

setRegBit(ADC12_CTRL1,STOP0);      //0x4000: Stop command issued

 

 

setRegBit(ADC12_PWR,APD);//Activa autoapagado
clrRegBits(ADC12_PWR2,ADC12_PWR2_SPEEDA_MASK);//relojA <5MHz
setRegBitGroup(ADC12_CTRL1,SMODE,0b101);//0x0005: triggered parallel
setRegBit(ADC12_CTRL1,EOSIE0);//0x0800: ADCA EOSI0 interrupt enabled
setRegBit(ADC12_CTRL1,SYNC0);//0x1000: ADCA Triggered by SYNC0 pulses

 

 

clrRegBit(ADC12_CTRL2,SIMULT);//0x0000: Independent
setRegBitGroup(ADC12_CTRL1,CHNCFG_L,0x03);//0x0030
setRegBitGroup(ADC12_CTRL2,CHNCFG_H,0x03);//0x00B0

 

 

clrRegBit(ADC12_CTRL1,STOP0);      /* Stop command cleared */

 

 

Best regards

Labels (1)
0 Kudos
Reply
4 Replies

2,042 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Carlos,

Firstly, all analog channel's allowed voltage are from GND to 3.3V, the analog channel pins ANAx or ANBx can not accept negative voltage from hardware perspective.

Secondly, I suggest you use Simultaneous mode by setting the SIMULT bit in ADC0_CTRL2.

Pls have a try, if there is still have abnormal digital sample, update the community page.

setRegBit(ADC12_CTRL2,SIMULT);//0x0000: simultaneous mode

BR

Xiangjun Rong

0 Kudos
Reply

2,042 Views
cabl
Contributor III

Dear Xiangjun,

thank you very much for the answer. However, I can see the point of using simultaneous mode if I´m not sampling any ADCB channels. More over when there are certain issues with ADCs power consumption.

By the way, I´ll give a try to the simultaneous mode.

BR

0 Kudos
Reply

2,042 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,Carlos,

what is the result, any progress?

BR

XiangJun Rong

0 Kudos
Reply

2,042 Views
cabl
Contributor III

Dear Xiangjun,

this strange behaviour appears once in a while, so I need days to be sure whether every change takes effect or not.

I´ll keep you informed.

Thanks again.

0 Kudos
Reply