SC18IS606 puts 1 in every 7e bit of a byte

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SC18IS606 puts 1 in every 7e bit of a byte

跳至解决方案
2,955 次查看
DannyEngeringh
Contributor III

Hello everyone, 

I'm trying to use a SC18IS606 incombination with a BGT60UTR. Writing the registers seems to work. but when i try to read back the register values. the SC18IS606 puts a one in every 7e bit of a byte. On the logic analyzer I see the right values coming by. but reading them seems not to work properly. 

I hope somebody can help. 

Regards

标记 (1)
0 项奖励
回复
1 解答
2,926 次查看
DannyEngeringh
Contributor III

Hi guoweisun, 

Thanks for your reply, The problem was caused by my raspberry-pi. do not realy understand why but with a different processor the problem was solved. 

regards

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,930 次查看
guoweisun
NXP TechSupport
NXP TechSupport

HI Danny:

Thanks for your interest in NXP  Products.

You can see below read command format:

guoweisun_0-1731563793086.png

guoweisun_2-1731564445507.png

 

You can see above read command for instance.

Thanks!

 

 

0 项奖励
回复
2,927 次查看
DannyEngeringh
Contributor III

Hi guoweisun, 

Thanks for your reply, The problem was caused by my raspberry-pi. do not realy understand why but with a different processor the problem was solved. 

regards

0 项奖励
回复