SC16IS752 TX FIFO not registering data from MCU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SC16IS752 TX FIFO not registering data from MCU

1,873件の閲覧回数
alberthchau
Contributor I

Hi,

I currently have an interface between my MCU (56F8357) and a SPI-to-UART bridge (SC16IS752) setup. I'm using SPI to send a byte of information from the MCU to the bridge. Here's my problem: when I write a char variable to the Transmit Holding Register (THR) in the bridge, I do not see the TXLVL register updating to show that I've added a byte of information to the transmit FIFO. I can see the byte of information on my oscilloscope as it moves out of the MOSI line between the MCU and bridge so the data is definitely sending - but just not registering into the FIFO for some reason

I've tried forcing the RTS to active (and make sure CTS is active high as well) to see if something sends out of the TX line on the SC16IS752 but nothing comes out of it. Here's what I have enabled in my registers:

FCR: TX FIFO reset, RX FIFO reset, FIFO enable

IER: RX data available niterrupt

LCR; divisor latch enable, parity enable, stop bit, word length bit 1 and 0

I've also tried my setup with Auto-CTS and Auto RTS on and off in the EFR register but to no avail.

Thanks for reading and any help would be greatly appreciated!

Al

タグ(5)
0 件の賞賛
返信
1 返信

1,618件の閲覧回数
david_diaz
NXP Employee
NXP Employee

Hello Albert,

Please review the application note from the link below. This document shows the SC16IS752 initialization in order to send and receive data, more specifically at chapter 6. I recommend to compare it with your initialization procedure.

 

Interfacing NXP bridge IC with NXP ARM microcontroller

 

Please let me know if you have any further question.

Regards,

David

0 件の賞賛
返信