SAA7706H audio input selection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SAA7706H audio input selection

2,108件の閲覧回数
svatonaspol
Contributor I

Good afternoon,

I have question regarding to the DSP controller SAA7706H, which is processing audio signal and is installed in variety of car stereos. I need to set the TAPE analog input as active and I did not find any reference regarding to the i2c memory map and what exact bytes must be set via I2c to activate the input. Is there any other reference, which is describing particular bits in each register? 

Thank you.

ラベル(1)
タグ(4)
0 件の賞賛
返信
0 返答(返信)