Repeat LIN failure with TJA1020

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Repeat LIN failure with TJA1020

2,181 次查看
mike8
Contributor I

Hello. I'm just a mechanic trying to fix a problem car, but here's the story.

I have a vehicle that has had a repeat failure of the LIN bus. This has required the cluster to be replaced each time to get LIN communication active. In less than a year, it has gone through 4 clusters and now they're discontinued. Each time I get the vehicle back, the LIN is "stuck" at about 1V. With every cluster, scoping the LIN circuit out of the cluster did not show any voltage spikes that may harm the circuit while manipulating everything controlled on the LIN bus. In our world, all trouble shooting would point towards replacing the cluster, but I know that won't last. I am looking for any insight as to what might take the LIN bus down. I have connected an IC test clip directly to the chip and checked all eight legs for something abnormal. The chip on this board is a TJA1020. The Vsup and NWake signals mirror each other with key on and start up and follow battery voltage. GND stays at 0V. TXD has a 5V pull up pattern, repeating (about 2 sec) with a break. Just before the break in TXD, both RXD and EN will signal at the same time like a synchronizer signal. RXD is a 5V pull up and EN is a 5V pull down.

Other than a voltage over spike, what could stop the chip from producing a signal on the LIN circuit? Does the NWake circuit need a signal (like a ground pulse) to get the chip operating? Would a low voltage on Vsup (like a bad battery during engine cranking) cause a failure?

Thanks for any input.

Mike

标记 (1)
0 项奖励
回复
1 回复

2,111 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Please down load TJA1020 datasheet for review before debug this part.

NWake pin is the local wake up pin (active low)which can wake up chip from sleep mode.

 VBAT normal range from 5V to 27V and typical 12V ,if out of this range this chip can't work well.

0 项奖励
回复