Quadrature Output Pulse Generation using Timers with 56F82748

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Quadrature Output Pulse Generation using Timers with 56F82748

2,525件の閲覧回数
sandeepn
Contributor II

How Can i generate Stream of Pulses(based on the speed at which my motor is spinning) which are to be quadrature in nature with Timers (Say Timer 0 & 1) with DSC 56F82748VLL. Also, Change the direction of Pulses based on the Direction of rotation. (This function is same as emulated encoder pulses. But to be generated from MCU) .

0 件の賞賛
返信
2 返答(返信)

2,436件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Sandeep,

I think you can use eFlexPWM module to generate the two signal with 90 degree shift, as the eFlexPWM has the function to generate the Phase Shifted PWMs.

I think you can use quadtimer to generate the two signal with 90 degree shift, when one timer is master, the other is slave. But it is easier to use eFlexPWM module.

Hope it can help you

B R

Xiangjun Rong

0 件の賞賛
返信

2,319件の閲覧回数
manikandanb
Contributor II

How to generate Quadrature output pulse using eflex pwm with DSC MC56F8247 controller using CodeWarrior v10.6.

0 件の賞賛
返信