Problem with TWR mc56f8257

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with TWR mc56f8257

2,277件の閲覧回数
jansimurda
Contributor I

Hi, I have a problem with my processor mc56f8257.

Description: - I uploaded a new program

                  - I launched debug mod

                  - I accidentally pressed the reset button

Since then, the board is frozen and can not communicate, but it is to load a new bootloader.

I use - USB cable to connect the MCU

        - Eclipse code warior

I attach a photo of the error message and I apologize for my English.

9407_9407.jpgchyba.JPG.jpg

 

 

 

 

Thanks for any tip.

 

 

Regards

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

2,111件の閲覧回数
sutter_zhou
NXP Employee
NXP Employee

Are you using CW10.4 or CW10.5? The best way is to refresh the firmware of JM60 on the TWR. If you're using a CodeWarrior whose version is older than 10.5, you can install CW10.5 and connect the board, it'll ask you to refresh the firmware through the bootloade when you dowload the code.


0 件の賞賛
返信