PWM module not triggering fault

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PWM module not triggering fault

5,932 Views
fasihahmed
Contributor IV

Have an issue that GPIO C14/C15 inputs are not enabling PWMs fault channels in GCT. Even though they are selected. im not able to get a check mark on the boxes

How can i manually enable them during initilisation process in main.c?

Im using MC56F837xx, CodeWarrior 11.1 and Quickstart 2.7

 

@xiangjun_rong 

 

 

fasihahmed_0-1605107473591.pngfasihahmed_0-1605107473591.png

fasihahmed_0-1605107672986.pngfasihahmed_0-1605107672986.png

 

0 Kudos
Reply
7 Replies

5,923 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Fasih,

Maybe it is only GCT tools issue. Pls output a PWM signal, and add the PWM_Fault signal, then observe the PWM signal and check if the Fault signal can disable PWM output.

Hope it can help you

BR

Xiangjun Rong

0 Kudos
Reply

5,920 Views
fasihahmed
Contributor IV

Can you tell me the code to manually enable/init the fault during startup? @xiangjun_rong 

im still not able to trigger an interrupt based on pwm faults

0 Kudos
Reply

5,900 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Fasih,

For example, the GPIOG_5 is multiplexed with PWMA_Fault3, you can use the code to enable fault function and generate fault interrupt.

/High logic of fault signal will disable PWM signal, The fault signal is inputed from the GPIOG5, the PWM signals recover after the Fault signal disappear
//automatically
void PWMAFault_GPIOG5(void)
{
//enable the GPIOG gated clock
SIM->PCE0|=1<<0;
//set the GPIOG5 bit in PER reg
GPIOG->PER|=0x20;
//set the GPIOG5 as PWMA fault3 signal
SIM->GPSGL&=~(0xC00);
SIM->GPSGL|=0x400;
}

//High logic of fault signal will disable PWM signal, The fault signal is inputed from the GPIOG5, the PWM signals recover after the Fault signal disappear
//automatically
void testFaultFunction(void)
{
//enable fault
SIM->IPS0&=~(0x08);
INTC->IPR8|=0x300;
PWMA->SM0DISMAP0=0x0088; //Disable PWMA_0A and 0B when the fault3 becomes high
PWMA->FCTRL0|=0x8808;
}

#pragma interrupt on
void PWMA_Fault_ISR(void)
{
//clear the PWMA_fault flag
PWMA->FSTS0|=0x088;
__asm(nop);
}
#pragma interrupt off

BR

Hope it can help you

0 Kudos
Reply

5,885 Views
fasihahmed
Contributor IV

the PWMs are disabled but i cannot get the ISR to trigger based on the PWM fault.

I use GPIOF5 and PWM_A_FL7

0 Kudos
Reply

5,875 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Fasih,

I see that the GPIOF5 pin can disable PWMA signal for your project, but can not generate interrupt, in the case, pls use the code.

But you have to add the PWMA_Fault_ISR to PWMA_fault interrupt vector table.

Hope it can help you

BR

XiangJun rong

void testFaultFunction(void)
{
//enable fault
INTC->IPR8|=0x300;
PWMA->SM0DISMAP1=0x0088; //Disable PWMA_0A and 0B when the fault3 becomes high
PWMA->FCTRL1|=0x8808;
}

 

#pragma interrupt on
void PWMA_Fault_ISR(void)
{
//clear the PWMA_fault flag
PWMA->FSTS1|=0x088;
__asm(nop);
}
#pragma interrupt off

0 Kudos
Reply

5,851 Views
fasihahmed
Contributor IV

fasihahmed_0-1606140804490.pngfasihahmed_0-1606140804490.png

 

in GCT's SYS - System Support Control why cant I choose the fault pins for example on GPIOF5? It only shows GPIO G's faults. Which are not supported by my DSC type. I need to select them on GPIOC14, GPIOC15 and GIPIOF5

 

Also in SYS.h im not able to find register for GPIOF5.

The below code shows for GPIOG5. How can i select the register for GPIOF5? 

//enable fault
SIM->IPS0&=~(0x08);

0 Kudos
Reply

5,830 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Fasih,

For the PWMA module of MC56F83xxx, there are 8 Faults pins, they are Fault 0/1/2/3 and Fault 4/5/6/7, for the Fault 0/1/2/3, there are TWO sources, one is from external pads, another is from crossbar, which one functions as Fault is dependent on the SIM->IPS0 register, that is why you are required to select the fault source for Fault 0/1/2/3 in SYS module.

For the Fault 4/5/6/7, there is only one source, external pads.

In conclusion, for fault 0/1/2/3, if you use external pads as fault pins, you are required to configure the SYS module and GPIO module, for example GPIO E8/E8 and G4/G5.

For the Fault 4/5/6/7, you are only required to set up the GPIO for example GPIO F4/F5..

Hope it can help you

BR

XiangJun Rong

 

0 Kudos
Reply