PWM MC56F8367

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PWM MC56F8367

3,769件の閲覧回数
maxrotter
Contributor I


Hello,

i use a chip MC56F8367 and codewarriorV8.2 and i don't know making a pwm-signal in C.

Maybe does anybody know thw solution.

 

Thanks

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,407件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

I develop an example of PWM module based on MC56F8367EVM and CodeWarrior for DSP56800/E ver8.3 tools, pls refer to it. You can see PWM signal on J7 connector on the EVM.

0 件の賞賛
返信

2,407件の閲覧回数
ankur_kala
NXP Employee
NXP Employee

Hi Max,

You can also try following the below mentioned steps to get started.

Peripheral Example Applications for 56800/E
Overview
Processor Expert provides example applications for many peripherals included on 56800/E devices
How to get this software
These example applications are included as part of the CodeWarrior Development Studio for 56800/E Digital
Signal Controllers. Follow these steps:
1.Install CodeWarrior Development Studio for 56800/E Digital Signal Controllers
2.Launch CodeWarrior, and create new Processor Expert project
a.Select File > New menu
b.Select Processor Expert Examples Stationery
c.Type project name
d.Click OK
e.Select DemoApplications > HWBeans > select desired processor > select desired peripheral
f.Click OK
3.Generate application code by selecting Processor Expert > Generate Code menu
Detailed documentation
Documentation for this application is included as part of this example project. Expand Doc folder located
in the project window by clicking on the + icon next to the folder, and open desired file by double clicking it.

0 件の賞賛
返信

2,407件の閲覧回数
Robinwithu
Senior Contributor I

Hi Max,

Please see the link, may be useful.

https://community.freescale.com/thread/304151

Thanks and Rgards,

Robin

0 件の賞賛
返信