PTN3363 TMDS input voltage level

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PTN3363 TMDS input voltage level

1,481 Views
matteoconti
Contributor I

Hi,

I'm developing an application in which an HDMI signal needs to be shifted up from 1.8V to 3.3V. At page 18 of this document characteristics of PTN3363 are shown: could someone please confirm me that V_RX and V_RX_Diff level range will accept my HDMI input? I'm a bit afraid of what's said on the datasheet "PTN3363 operates only when the input signal level is above certain minimum threshold (as per VRX_DIFFp-p). If the input falls below that minimum threshold, the outputs are squelched."

Thank you very much,

Regards,

Matteo

Labels (1)
0 Kudos
Reply
0 Replies