PTN3363 TMDS input voltage level

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PTN3363 TMDS input voltage level

1,498 次查看
matteoconti
Contributor I

Hi,

I'm developing an application in which an HDMI signal needs to be shifted up from 1.8V to 3.3V. At page 18 of this document characteristics of PTN3363 are shown: could someone please confirm me that V_RX and V_RX_Diff level range will accept my HDMI input? I'm a bit afraid of what's said on the datasheet "PTN3363 operates only when the input signal level is above certain minimum threshold (as per VRX_DIFFp-p). If the input falls below that minimum threshold, the outputs are squelched."

Thank you very much,

Regards,

Matteo

标签 (1)
标记 (3)
0 项奖励
回复
0 回复数