PCA9698DGG maximum toggling frequency

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PCA9698DGG maximum toggling frequency

1,529 次查看
Blessing
Contributor I

Dear team,

We are using PCA9698DGG in our design, we are planning to use the mentioned component to drive a clock frequency of about 30 Mhz and receive the same.Kindly provide the max. & min recommended Tx and Rx frequency limit for the mentioned component.

Regards,
Blessing Selvakumar,
Hardware Design Engineer.

4 回复数

1,398 次查看
jennie258fitz
Contributor II

Thank you for helping people get the information they need. Great stuff as usual. Keep up the great work!!! NYStateofHealth

0 项奖励
回复

1,505 次查看
Blessing
Contributor I

Hi Guoweisun,

Yes,I need to know whether PCA9698 will be able to generate a toggling data / clock at frequency <30 Mhz and able to receive the same if provided as input.

0 项奖励
回复

1,435 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Hi 

30MHZ is not possible for this part,the IIC supported speed maximum is 1MHZ.

0 项奖励
回复

1,516 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Hi 

Do you mean to use PCA9698 generate 30MHz PWM/clock signal?

 

0 项奖励
回复