PCA9698DGG maximum toggling frequency

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA9698DGG maximum toggling frequency

3,277 Views
Blessing
Contributor I

Dear team,

We are using PCA9698DGG in our design, we are planning to use the mentioned component to drive a clock frequency of about 30 Mhz and receive the same.Kindly provide the max. & min recommended Tx and Rx frequency limit for the mentioned component.

Regards,
Blessing Selvakumar,
Hardware Design Engineer.

4 Replies

3,146 Views
jennie258fitz
Contributor II

Thank you for helping people get the information they need. Great stuff as usual. Keep up the great work!!! NYStateofHealth

0 Kudos
Reply

3,253 Views
Blessing
Contributor I

Hi Guoweisun,

Yes,I need to know whether PCA9698 will be able to generate a toggling data / clock at frequency <30 Mhz and able to receive the same if provided as input.

0 Kudos
Reply

3,183 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi 

30MHZ is not possible for this part,the IIC supported speed maximum is 1MHZ.

0 Kudos
Reply

3,264 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi 

Do you mean to use PCA9698 generate 30MHz PWM/clock signal?

 

0 Kudos
Reply