PCA9698DGG is not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PCA9698DGG is not working

1,805 次查看
JHKIM7
Contributor I

Hi ALL

I am evaluating PCA9698DGG, but PCA9698DGG is not working.

You can see the waveform and schematic as like below.

JHKIM7_0-1622263581026.png

 

The waveform capture conditions are below.

  1. SCL frequency : 400KHz
  2. Slave address 0x4E
  3. Command register : 0x08
  4. Data : 0xFF
  5. OE pin : GND
  6. MCU : ATMEGA128

JHKIM7_2-1622263642040.png

 

 

Some strange thing is that SDA signal is very fast drop down after received ACK.

Also, I had changed SCL frequency and Slave address, but result is same.

Could you please help this issue?

Best regards.

JH Kim

标记 (1)
0 项奖励
回复
4 回复数

1,755 次查看
JHKIM7
Contributor I

Hi

Regarding to datasheet, output enable when OEPOL = 1.

But in my case, output enable when OEPOL = 0

Is PCA9698DGG datasheet correct on OEPOL and OE Pin?

 

Thanks

JH Kim

0 项奖励
回复

1,740 次查看
guoweisun
NXP TechSupport
NXP TechSupport

OEPOL bit controls the polarity of OE pin.
– OEPOL = 0: OE pin is active LOW.
– OEPOL = 1: OE pin is active HIGH (equivalent to OE pin).

when OEPOL set to 0,low OE active.

0 项奖励
回复

1,768 次查看
JHKIM7
Contributor I

Hi 

The pull up resistors are located at MCU side. The value is 1.5Kohm.

I think normal working I2C, but PCA9689 output is "0" level under below condition.

  1. SCL frequency : 400KHz
  2. Slave address 0x4E
  3. Command register : 0x08
  4. Data : 0xFF
  5. OE pin : GND
  6. MCU : ATMEGA128

I think PCA9689 output is high level under upper condition.

I don't know what's wrong with no output.

Could you please adivce?

Thanks,

JH Kim

0 项奖励
回复

1,790 次查看
guoweisun
NXP TechSupport
NXP TechSupport

1: What's the result when your drop down the frequency?

2:what's the pull up resistors of SDA/SCL of PCA8698?

0 项奖励
回复