PCA9698 ERROR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PCA9698 ERROR

1,600 次查看
shoujian_lv
Contributor I

HI

I use PCA9698 to solve the problem of insufficient IO port.

But there are problems in the use process:

I use the IO of pca9698 to control the digital switch(ADG1612),when the control port of the digital switch is not connected to the IO port of pca9698,i can control the IO as i want.

But when more than 4 control ports of the digital switch are  connected to the IO port of pca9698(these ports is in one register),and IO is configured as output,if set these ports(more than 4 ports) HIGH at same time,Configuration registers corresponding to these ports will be configure as input. In this case, it is invalid to configure IO as output.

标记 (1)
0 项奖励
回复
1 回复

1,521 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Please also provide schematic!

0 项奖励
回复