Need information regarding cell controller BMS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need information regarding cell controller BMS

1,682 Views
pratayay123
Contributor III

Dear Team,

As per the Application note for MC33772B Passive cell balancing also included inside the Evaluation board. please replay the below query.

1. Is it possible to get only the sensing module without the passive balancing?

2. Even if passive balancing included with the controller ..is it possible to bypass the passive balancing section?

3. is there any NXP board available for Active cell balancing?

4. Is there any module for lithium-ion battery voltage, current, and temperature sensing?

Thanks,

Pratyay

0 Kudos
Reply
1 Reply

1,658 Views
guoweisun
NXP TechSupport
NXP TechSupport

For your questions the answer are NO.

0 Kudos
Reply