NVT2010 problems in the process of use

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NVT2010 problems in the process of use

2,082 Views
Geekpink
Contributor I

Vpu(A)=1.1V, Vpu(B)=1.8V, Vpu(H)=3.3V;

The EN and VREFB pin inputs are 3.3V, but the B side pulls up to 1.8V, is this allowed? Are there any risks associated with this use?

 

0 Kudos
Reply
2 Replies

2,049 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Yuliang,

It should work in this configuration. 

BRs, Tomas

0 Kudos
Reply

2,081 Views
Geekpink
Contributor I

Geekpink_0-1716386585783.png

The usage is shown in the image above

 

0 Kudos
Reply