NVT2010 problems in the process of use

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NVT2010 problems in the process of use

2,015件の閲覧回数
Geekpink
Contributor I

Vpu(A)=1.1V, Vpu(B)=1.8V, Vpu(H)=3.3V;

The EN and VREFB pin inputs are 3.3V, but the B side pulls up to 1.8V, is this allowed? Are there any risks associated with this use?

 

0 件の賞賛
返信
2 返答(返信)

1,982件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Yuliang,

It should work in this configuration. 

BRs, Tomas

0 件の賞賛
返信

2,014件の閲覧回数
Geekpink
Contributor I

Geekpink_0-1716386585783.png

The usage is shown in the image above

 

0 件の賞賛
返信