Most recent version of DSP56000 development tools

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Most recent version of DSP56000 development tools

7,377件の閲覧回数
sascha_springer
Contributor I

Does anyone know the most recent version numbers (MS-DOS, Windows, Solaris, Next, Atari ST) of the DSP56000 development tools like from the Suite56? I know that there are some related tool download links here for the DSP56300 and DSP56600 devices but I don't know if these assemblers are compatible with the DSP56001.

ラベル(1)
タグ(2)
0 件の賞賛
返信
6 返答(返信)

5,623件の閲覧回数
Cyndanera
Contributor I

Hi do you have the DSP56000 latest dev tools for the Windows NT version?

タグ(2)
0 件の賞賛
返信

7,283件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Sascha,

I attach the tools for DSP56000 family, including the assembly compiler and debugger.

Hope it can help you.

BR

XiangJun Rong

0 件の賞賛
返信

7,284件の閲覧回数
sascha_springer
Contributor I

Thanks XiangJun for the fast reply. Unfortunately, however, it seems that the archive is missing some files. I was expecting ASM56000.EXE and CLDLOD.EXE in the package but I cannot find them.

0 件の賞賛
返信

7,284件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Sascha,

Pls refer to this package, it includes the asm56000.exe.

BR

XiangJun Rong

7,284件の閲覧回数
sascha_springer
Contributor I

Thanks! That's the one I was looking for.

The version of the assembler is 6.3.0. It's running under Windows which is fine so far. I suppose that the versions for other architectures didn't survive!?

0 件の賞賛
返信

7,284件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Sascha,

Yes, we have not all version of the tools. For the other architecture, it is case by case for the processor which is end of life.

BR

XiangJun Rong

0 件の賞賛
返信