[MWCT2013]PWM Control

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[MWCT2013]PWM Control

Jump to solution
3,371 Views
RichardT
Contributor I

Dear NXP,

 

Could anyone provide about the PWM initial and control code for pin 45, 46, 51?

I have to control each pin to output the PWM function individually.

 

Thnak you.

0 Kudos
Reply
1 Solution
3,329 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi

Pls refer to the code, which can be used for the MWCT2013 I suppose

BR

XiangJun Rong

View solution in original post

0 Kudos
Reply
3 Replies
3,335 Views
RichardT
Contributor I

Dear XiangJun,

 

unfortunately, it did not work properly after I read this document.

I still want to have sample code for MWCT2013.

 

Thank you.

0 Kudos
Reply
3,330 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi

Pls refer to the code, which can be used for the MWCT2013 I suppose

BR

XiangJun Rong

0 Kudos
Reply
3,340 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you know that the MWCT2013 has application code for wireless charging, so you have to check if the application code has used the pin pin 45, 46 and 51. If the three pins are not used, you can develop code to use them.

This link has eFlexPWM application code, pls refer to it.

https://community.nxp.com/t5/Digital-Signal-Controllers/Two-or-more-eFlexPWM-synchronization-for-KV4...

 

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply