[MWCT2013]PWM Control

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[MWCT2013]PWM Control

ソリューションへジャンプ
3,434件の閲覧回数
RichardT
Contributor I

Dear NXP,

 

Could anyone provide about the PWM initial and control code for pin 45, 46, 51?

I have to control each pin to output the PWM function individually.

 

Thnak you.

0 件の賞賛
返信
1 解決策
3,392件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi

Pls refer to the code, which can be used for the MWCT2013 I suppose

BR

XiangJun Rong

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,398件の閲覧回数
RichardT
Contributor I

Dear XiangJun,

 

unfortunately, it did not work properly after I read this document.

I still want to have sample code for MWCT2013.

 

Thank you.

0 件の賞賛
返信
3,393件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi

Pls refer to the code, which can be used for the MWCT2013 I suppose

BR

XiangJun Rong

0 件の賞賛
返信
3,403件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you know that the MWCT2013 has application code for wireless charging, so you have to check if the application code has used the pin pin 45, 46 and 51. If the three pins are not used, you can develop code to use them.

This link has eFlexPWM application code, pls refer to it.

https://community.nxp.com/t5/Digital-Signal-Controllers/Two-or-more-eFlexPWM-synchronization-for-KV4...

 

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信