MPC56F837xx_Cust:Aptera_16 independent PWMs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC56F837xx_Cust:Aptera_16 independent PWMs

1,837 Views
jbirchy
Contributor IV

 

How do we get 16 independent PWMs on a MC56837xx device?

It looks like we can use A and/or B and/or X from the submodule, but how?   Is that documented anywhere?

We also must use the 100 LQFP to get 16 PWM output channels also, the 80 LQFP only supports 14 channels, correct?

Thanks

John

0 Kudos
Reply
2 Replies

1,833 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, John,

I think it is okay to use 100 pin or 80 pins MC56F83xxx to output independent PWM signals.

As you know that the MC56F83xxx has two eFlexPWM modules: eFlexPWMA and eFlexPWMB, each eFlexPWM module has 4 sub-module. Each PWM sub-module can output two PWM signals:PWM_xA, PWM_xB, the two PWM signals PWM_xA, PWM_xB have the same frequency.

So the eFlexPWMA can output 8 PWM signals:PWMA_0A/0B,PWMA_1A/1B,PWMA_2A/2B,PWMA_3A/3B.

The eFlexPWMB can output 8 PWM signals:PWMB_0A/0B,PWMB_1A/1B,PWMB_2A/2B,PWMB_3A/3B.

They can output 16 PWM signals totally.

Pls refer to section 10.1 MC56F83xxx Signal Multiplexing and Pin Assignments in data sheet of MC56F83xxx.

I have checked that for 80 pin package, all 8 PWM signals for PWMA module can output from pins.

Pin index(80 LQFP)                        PWM signals

55                                                    PWMA_0B

56                                                     PWMA_0A

57                                                     PWMB_0B

58                                                     PWMB_0A

59                                                     PWMA_1B

60                                                      PWMA_1A

63                                                      PWMB_1B

64                                                      PWMB_1A

65                                                      PWMA_2B

66                                                      PWMA_2A

67                                                      PWMA_3B

68                                                     PWMA_3A

 

The PWMB_2A/2B, PWMB_3A/3B can not output to pad directly, but you can output them from crossbar.

As the following crossbar fig, you can output the PWM signals from the crossbar package pins:

xiangjun_rong_0-1624602021404.png

 

xiangjun_rong_1-1624602202854.png

You can set up the PWM Output Trigger Control Register to have the trigger signal to output PWM signal.

Pls refer to section 27.3.22 Output Trigger Control Register (SM0TCTRL - SM3T
CTRL)
Hope it can help you

BR

XiangJun Rong

 

 

 

 

0 Kudos
Reply

1,806 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls refer to the doc for the application that you use crossbar to output PWM signals.

https://community.nxp.com/t5/Digital-Signal-Controllers/Route-the-PWM-signals-to-external-pad-via-cr...

 

BR

XiangJun Rong

0 Kudos
Reply