MC56F84xxx of ADC processor expert setting question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC56F84xxx of ADC processor expert setting question

ソリューションへジャンプ
1,601件の閲覧回数
Kris_Ke
Contributor III

Hi  

The datasheet show the 12-bit ADC frequency is 20Mhz.

frequency.PNG

When I setting the processor expert of the ADC, it always show "Warning : A/D frequency is too fast" and "Warning : A/D frequency 1 is too fast"

adc.PNG

 

No matter how you change the frequency, this warning will not disappear.

Did I miss anything that I didn’t set?

 

 

Thanks,

Kris

タグ(1)
0 件の賞賛
返信
1 解決策
1,592件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Kris,

I have tested to try to input different value for the "Clock divisor select value" box, the "warning: A/D frequency is too fast" always appears, so I think it is a bug of the PE for MC56F84xxx for CodeWarrior for mcu ver11.x.

Pls do not care about it.

BR

XiangJun Rong

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,593件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Kris,

I have tested to try to input different value for the "Clock divisor select value" box, the "warning: A/D frequency is too fast" always appears, so I think it is a bug of the PE for MC56F84xxx for CodeWarrior for mcu ver11.x.

Pls do not care about it.

BR

XiangJun Rong

0 件の賞賛
返信