MC56F83783 Flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC56F83783 Flash

1,575件の閲覧回数
547351265
Contributor II

The 83XXX Flash block is divided into two sections, block0 and block1. Now put the black box in the block0. When you switch to the block1, the black box will not be used.Should the black box program also have its counterpart in Block1?Or do you call the black box program in a public section?

0 件の賞賛
返信
1 返信

1,568件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, HZ,

I suppose you mean the flash programming mechanism, there is Flash memory Module(FTFE), it's register address is located at the X:1c7xx, with the register operation, you can erase/program the block0 and block1.

This is the part of FTFE register.

xiangjun_rong_0-1614139645534.png

If I misunderstand you, I am sorry.

BR

XiangJun Rong

 

0 件の賞賛
返信