MC56F8355 start up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC56F8355 start up

1,915件の閲覧回数
christophe_c
Contributor I

Hello,

I use an MC56F8355 and it doesn't start when I heat it.

The RESET signal is OK but the RSTO signal stayes at 0.

Thank you for your help

Regards

Christophe

0 件の賞賛
返信
3 返答(返信)

1,885件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that the MC56F8355 can run if you don't heat it.

This is the ambient temperature range the MC56F8355 can work.

Hope it can help you

BR

XiangJun Rong

xiangjun_rong_0-1694747827480.pngxiangjun_rong_0-1694747827480.png

 

0 件の賞賛
返信

1,858件の閲覧回数
christophe_c
Contributor I

Hi,

 

If the temperature is 25°C, it's OK.

If the temperature is 10°C or 50°C, it's not OK.

I changed crystal by a ceramic resonator 8MHz and I can start the µcontroller at 10 and 50°C.

Is it necessary to change the bit  register COHL which is at  1.

Regards

 

Christophe

 

0 件の賞賛
返信

1,835件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

If you use 8MHz ceramic resonator, I suppose the COHL bit should be cleared.

Pls refer to section 5.11.5 Oscillator Control Register w/o Relaxation Oscillator (OSCTL) in MC56F8300UM.pdf

Hope it can help you

BR

XiangJun Rong

xiangjun_rong_0-1695021726375.pngxiangjun_rong_0-1695021726375.png

 

0 件の賞賛
返信