MC56F82748 connection failure by Multlink Universal Rev B

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC56F82748 connection failure by Multlink Universal Rev B

2,114 Views
admin
Specialist II

Original Content posted by Li Yang 

 


We find MC56F82748 connection failure by Multilink Universal Rev B, if using Multilink Universal Rev A and Rev C, no such issue. We try to update the firmware of Rev B, it has no effect. Is there a way to solve the issue?

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,882 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Yang

I’m using Multilink Universal Rev B to program MC56F82748, and have no problem.

Could you please create a new bareboard project for MC56F82748, and do not add your own application code, then debug again with P&E Universal Multilink, does it work well?

If not, please open the Project Properties and go to ‘Run/Debug Settings’, please check whether the Multilink Universal is recognized as below.  If not, please click on ‘FAQ#29’ to check the driver installation. 

The latest driver and firmware can be downloaded from:

http://www.pemicro.com/support/downloads_find.cfm

Hope this helps! If not, I would suggest submitting an issue on the P&E forum:

http://www.pemicro.com/forums/index.cfm

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,882 Views
mohammad_kamil
NXP Employee
NXP Employee

Hi Li Yang,

can you please raise ticket with PE micro, As it seems this issue is with Multilink software and not DSC.

0 Kudos
Reply