MC56F82748 Internal Flash configuration problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC56F82748 Internal Flash configuration problem

ソリューションへジャンプ
3,227件の閲覧回数
terrybogard
Contributor II

Dear NXP expert,

I found if i set the WAIT IN RAM --Yes. my program will run out of control if I declare an array[64], but is declare an array[32] is OK. and I set WAIT IN RAM --No. the program will run well. Can you give me some explain? my opinion is the stack overflow. And any suggestion about WAIT IN RAM item will be welcome.

Thanks.

 

Screenshot 2021-12-03 162121.png

0 件の賞賛
返信
1 解決策
3,214件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As the following figure and the "WAIT IN RAM" explanation, if you select "WAIT IN RAM" as Yes, it is in polling mode, in other words, the function polls the flash status register and checks if the flash operation is complete.

If you select "WAIT IN RAM" as No, it is in interrupt mode, in other words, after the flash operation is over, an flash interrupt is triggered, and the ISR will be executed, in the ISR, the flash status variable is updated. The advantage of the method is that you can execute the other function while the flash is operated.

Hope  it can help you

BR

XiangJun Rong

xiangjun_rong_0-1638774461646.png

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,226件の閲覧回数
terrybogard
Contributor II

when I set the WAIT IN RAM --No, the data write into internal Flash is wrong.

0 件の賞賛
返信
3,215件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As the following figure and the "WAIT IN RAM" explanation, if you select "WAIT IN RAM" as Yes, it is in polling mode, in other words, the function polls the flash status register and checks if the flash operation is complete.

If you select "WAIT IN RAM" as No, it is in interrupt mode, in other words, after the flash operation is over, an flash interrupt is triggered, and the ISR will be executed, in the ISR, the flash status variable is updated. The advantage of the method is that you can execute the other function while the flash is operated.

Hope  it can help you

BR

XiangJun Rong

xiangjun_rong_0-1638774461646.png

 

0 件の賞賛
返信