MC56F8006 - Low Frequency PWM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC56F8006 - Low Frequency PWM

2,106件の閲覧回数
CarlosCba
Contributor II

Dear,

 

Is possible to achieve a 10Hz frequency in the PWM module?

If is it possible, which are the correct settings?

 

Thanks.

ラベル(1)
0 件の賞賛
返信
1 返信

1,968件の閲覧回数
johnlwinters
NXP Employee
NXP Employee


The general answer is of course this can be done.  However, what is the clock frequency you are running the system at?

It can be set to a very low frequency to save power.

HOW to do this will depend on what else you are doing at the same time; the complete system view would help, or as much as you can share.

If you wish to keep such confidential, I suggest using the technical information center support available at www.freescale.com.