MC56F8006 - Low Frequency PWM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC56F8006 - Low Frequency PWM

2,099 Views
CarlosCba
Contributor II

Dear,

 

Is possible to achieve a 10Hz frequency in the PWM module?

If is it possible, which are the correct settings?

 

Thanks.

Labels (1)
0 Kudos
Reply
1 Reply

1,961 Views
johnlwinters
NXP Employee
NXP Employee


The general answer is of course this can be done.  However, what is the clock frequency you are running the system at?

It can be set to a very low frequency to save power.

HOW to do this will depend on what else you are doing at the same time; the complete system view would help, or as much as you can share.

If you wish to keep such confidential, I suggest using the technical information center support available at www.freescale.com.