MC5684565 reset lock-up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC5684565 reset lock-up

1,823 Views
kendegrave
Contributor I

I have a condition at 95 degree C ambient where a TLV803S is connected to the reset pin 2 of a Freescale MC5684565 uC with a 10K pull up to 3.3v and a 0.1uF pull down to ground which some times lock to a 600mV level.

If I bring the temperature to room it still is at this level.

If I remove power and re-energize it still stays at this level.

If the reset line is shorted to ground and opened, it stays at this level.

If the reset line is shorted to 3.3 volts and opened, the reset line now operates normally.

At this moment in time we do not know what triggers this condition.

We do not know if it is the supervisor or the uC.

We are currently doing non-evasive testing before we can start physically altering the node.

Dose anyone have any ideas what this may be?

 

Ken DeGrave

Labels (1)
0 Kudos
Reply
1 Reply

1,455 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Ken,

I think the 0.1uF capacitor in unnecessary, how about removing it?

BR

XiangJun Rong

0 Kudos
Reply