MC33790

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC33790

3,681件の閲覧回数
MNRH
Contributor I

Hi,

We are using the MC33790 for establishing an a DSI1.0 communication with a sensor module MC33793

As per the document we have provided the circuit with the VCC as 5V and Vsup as 24V while sending the data the Idle voltage is coming only up to 11.5V, not 24V can someone explain to me why the idle voltage is not reaching the expected 24V. 

Thanks 

Rakesh 

0 件の賞賛
返信
6 返答(返信)

3,537件の閲覧回数
MNRH
Contributor I

RakeshHegden_0-1656486130090.png

 

0 件の賞賛
返信

3,597件の閲覧回数
MNRH
Contributor I

Hi,

It was an issue with the DSIxF and DSIxS pin status if it is 1,0 respectively this issue occurs if it is set to 1,1 the VIDLE goes to 24V.

No it's not working with the MC33793 even after fixing the V Idle voltage issue  

 

0 件の賞賛
返信

3,648件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Does it work well if Vsup down to 11.5V?

0 件の賞賛
返信

3,537件の閲覧回数
MNRH
Contributor I

No, It won't work 

0 件の賞賛
返信

3,532件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

So your company is Dorman Products, right?

0 件の賞賛
返信

3,570件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport
Please show your schematic here!
0 件の賞賛
返信