Is it possible for the HCS12 XGATE to read two parallel lines of data?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible for the HCS12 XGATE to read two parallel lines of data?

704 Views
danbocko
Contributor I

I am using an ADC that has two Data Outputs (DO and D1). Ch0 - Ch3 are output on D0 and Ch4 - Ch7 are output on D1 The maximum DCLK would be 32.768 MHz and the maximum Output Data rate would be 64KHz. Is it possible that the XGATE could read the simultaneous data on D0 and D1? Each data stream is 128 bits deep (4 channels * 32 bits per channel) The image below is the output using DCLK of 2.048MHz. If this can be done with the XGATE, is there an AP Note or something to get started.

Thanks

Dan

DataOutput.jpg

Labels (1)
0 Kudos
Reply
0 Replies