Is Freemaster supported on the 56F8037?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is Freemaster supported on the 56F8037?

ソリューションへジャンプ
2,523件の閲覧回数
Larry5335
Contributor IV

Customer is having issues getting Freemaster to work with a 56F8037. Is a serial or CAN connection recommended?

What versions of CodeWarrior  are compatible with both?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,333件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Freemaster supports  the connection with 56F8037 through JTAG or SCI interface.

User can use either Classic CodeWarrior v8.3 or Eclipse  CodeWarrior v10.6  to develop the application which supports Freemaster connection.

Processor Expert contains two beans for FreeMaster communication, one is PC_Master, the other is FreeMaster. For SCI connection, you can choose either of them. For JTAG connection (using parallel or USBTAP), you can only choose FreeMaster.

Best Regards

Fiona

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,334件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Freemaster supports  the connection with 56F8037 through JTAG or SCI interface.

User can use either Classic CodeWarrior v8.3 or Eclipse  CodeWarrior v10.6  to develop the application which supports Freemaster connection.

Processor Expert contains two beans for FreeMaster communication, one is PC_Master, the other is FreeMaster. For SCI connection, you can choose either of them. For JTAG connection (using parallel or USBTAP), you can only choose FreeMaster.

Best Regards

Fiona

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信