If TDA8954J supply ok, clock signal ok?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

If TDA8954J supply ok, clock signal ok?

6,278件の閲覧回数
zw_wuxv
Contributor I

Debug the module of TDA8954J, no clock signal(internal clock) , no output.

+/-41VDC supply.

0 件の賞賛
返信
2 返答(返信)

6,151件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

Please update your schematic with attached application note if any difference!

By the way this device had already EOL no recommend for new design or project.

0 件の賞賛
返信

6,151件の閲覧回数
zw_wuxv
Contributor I

Hi G.w. Sun:

The trouble is still about the TDA8954J, Boss had choosen the IC.So we must finish the project.

There are 4 questions:

1)the led2 flickers when it has a 4OHM load(no signal input);

pastedImage_1.png

2)when output has a load(4ohm),the output wave is not so clear. the filter's parameters need to change?

pastedImage_2.png

3)What's your suggestions about the GND layout?

4)the crosstalk is big.

Can we contact with email?

0 件の賞賛
返信