Debug the module of TDA8954J, no clock signal(internal clock) , no output.
+/-41VDC supply.
Hi G.w. Sun:
The trouble is still about the TDA8954J, Boss had choosen the IC.So we must finish the project.
There are 4 questions:
1)the led2 flickers when it has a 4OHM load(no signal input);
2)when output has a load(4ohm),the output wave is not so clear. the filter's parameters need to change?
3)What's your suggestions about the GND layout?
4)the crosstalk is big.
Can we contact with email?