I did not compile "Hello World" .cpp code in MCUXpresso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I did not compile "Hello World" .cpp code in MCUXpresso

5,532 Views
pratikj_panchal
Contributor I

Hello,

I'm working in MCUXpresso IDE 11.0.
I'm working in .cpp source file and generate a file with GNU C++ 11(-std=gnu++11) Standard toolchain.

I want to Build and compile basic hello world code with this toolchain.
I also try to modify Newlib and NewlibNano Library header but not solve my issue yet.


#include
<iostream>

using namespace std;

int main()

{

cout << "Hello, World!";

return 0;

}

Above code I want to compile.When I compile this code I got an error(Please find Attachment).

Description    Resource    Path    Location    Type
'ECANCELED' was not declared in this scope    MIMXRT1062xxxxA_Project_CES_DEMO        line 126, external location: c:\nxp\mcuxpressoide_11.0.0_2516\ide\plugins\com.nxp.mcuxpresso.tools.win32_11.0.0.201905131304\tools\arm-none-eabi\include\c++\8.2.1\arm-none-eabi\thumb\v7e-m+dp\hard\bits\error_constants.h    C/C++ Problem
'ENOTRECOVERABLE' was not declared in this scope    MIMXRT1062xxxxA_Project_CES_DEMO        line 151, external location: c:\nxp\mcuxpressoide_11.0.0_2516\ide\plugins\com.nxp.mcuxpresso.tools.win32_11.0.0.201905131304\tools\arm-none-eabi\include\c++\8.2.1\arm-none-eabi\thumb\v7e-m+dp\hard\bits\error_constants.h    C/C++ Problem
'ENOTSUP' was not declared in this scope    MIMXRT1062xxxxA_Project_CES_DEMO        line 122, external location: c:\nxp\mcuxpressoide_11.0.0_2516\ide\plugins\com.nxp.mcuxpresso.tools.win32_11.0.0.201905131304\tools\arm-none-eabi\include\c++\8.2.1\arm-none-eabi\thumb\v7e-m+dp\hard\bits\error_constants.h    C/C++ Problem
'EOWNERDEAD' was not declared in this scope    MIMXRT1062xxxxA_Project_CES_DEMO        line 135, external location: c:\nxp\mcuxpressoide_11.0.0_2516\ide\plugins\com.nxp.mcuxpresso.tools.win32_11.0.0.201905131304\tools\arm-none-eabi\include\c++\8.2.1\arm-none-eabi\thumb\v7e-m+dp\hard\bits\error_constants.h    C/C++ Problem
make: *** [source/subdir.mk:49: source/MIMXRT1062xxxxA_Project_CES_DEMO.o] Error 1    MIMXRT1062xxxxA_Project_CES_DEMO             C/C++ Problem
make: *** Waiting for unfinished jobs....    MIMXRT1062xxxxA_Project_CES_DEMO             C/C++ Problem

How could I resolve this issue?
Kindly give me a way.

Regards,
Pratik Panchal


0 Kudos
Reply
2 Replies

5,158 Views
pratikj_panchal
Contributor I

Yes,you are right.
When we create a new project at that time lwip/errno.h have only a single file include #include "lwip/errno.h".
So, our compiler finds errno.h in system file but not included in lwip/errno.h.

So, just replace following snippet from lwip/errno.h

#ifndef __ERRNO_H__
#define __ERRNO_H__
#include "lwip/errno.h"
#ifndef __error_t_defined
typedef int error_t;
#define __error_t_defined 1
#endif

#include <sys/errno.h>

#endif /* !__ERRNO_H__ */

Thanks for Support.

0 Kudos
Reply

5,158 Views
houe
Contributor II

I ran into this issue as well. The problem was that lwip's version of <errno.h> was being included instead of the standard c++ library version of <errno.h>. By any chance are you compiling with #include path's from lwip?

0 Kudos
Reply