How to merge two srec files to one file to program to MC56F8246? one is bootloader, the other is application, we want to program it one time, so we must to merge two srec files to one?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to merge two srec files to one file to program to MC56F8246? one is bootloader, the other is application, we want to program it one time, so we must to merge two srec files to one?

3,057件の閲覧回数
huaping
Contributor III

one is bootloader, the other is application, we want to program it one time, so we must to merge two srec files to one?

Original Attachment has been moved to: bootloader.s.zip

Original Attachment has been moved to: application.s.zip

ラベル(1)
0 件の賞賛
返信
1 返信

1,828件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Dear Huaping Tian

56800E Flash Programmer can program with multiple S-record file, so you can program one time with the bootloader.s and application.s by 56800E Flash Programmer, but you must use its command line version, please see the section 2.1 for details in its help doc:
<install path>\Freescale\FlashProgrammer v1.2\Help\PDF\56800E_Flash-Programming.pdf

Best Regards

Fiona

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信