Helow, I'm in need of a development board to control power electronics circuits with IGBTs. What would be the most suitable for this type of application? Very thank you.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Helow, I'm in need of a development board to control power electronics circuits with IGBTs. What would be the most suitable for this type of application? Very thank you.

1,016 Views
jandersonduarte
Contributor I

Helow, I'm in need of a development board to control power electronics circuits with IGBTs. What would be the most suitable for this type of application? Very thank you.

Labels (1)
0 Kudos
Reply
1 Reply

886 Views
johnlwinters
NXP Employee
NXP Employee

The MC56F8200 Tower System 32-bit MCU module (TWR-56F8200) is an evaluation, demonstration and development board. The TWR-56F8200 can operate standalone or as the main control board in a Tower system with peripheral modules. It can also be used as the main control board with an APMOTOR56F8000E motor control board.

In the Tower system there are a large selection of boards to add to the evaluation configuration available at www.freescale.com.


0 Kudos
Reply