Hdmi lcd interface in NXP® i.MX 6SoloX processor using TDA19988 driver ic

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hdmi lcd interface in NXP® i.MX 6SoloX processor using TDA19988 driver ic

3,057 Views
hitenpchauhan
Contributor I

Hello,

I am using NXP® i.MX 6SoloX related board and I want to connect one 1024x600 hdmi touch screen display with it so I buy one display which is (https://www.waveshare.com/7inch-hdmi-lcd-c.htm )

Now my problem is when I read the datasheet of TDA19988 video driver ic I found Timing parameters for video supported table in the datasheet which has not to mention 1024x600 resolution option

So my question is TDA19988 is supported 1024x600 resolution or not? because I try so many things to connect this display to my board but not get any good results?

Thanks,

Labels (1)
0 Kudos
Reply
3 Replies

2,928 Views
hitenpchauhan
Contributor I

So you mean to say that 1024 x 600 lcd it may be working with my board + TDA19988  driver?

0 Kudos
Reply

2,928 Views
joanxie
NXP TechSupport
NXP TechSupport

yes, it should be work since imx6sx can support 1280x720 resolution

0 Kudos
Reply

2,928 Views
joanxie
NXP TechSupport
NXP TechSupport

1024x600 isn't the standard solution which current bsp can support, you need to know the panel timings parameter, then add them in the current bsp

0 Kudos
Reply