GDFLIB example for M0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GDFLIB example for M0

1,379 Views
donoldham
Contributor I

I am trying to use the GDFLIB with the MLIB libraries for a simple filter implemented on the MKE02, M0+ core.  Is there a full example of implementing a filter?  And how do I scale the fractional values back to an integer?

0 Kudos
Reply
1 Reply

1,293 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Don,

Regarding your question, as you know that the GDFLIB library is served for motor control, we have not the independent example. The filter function is used in the motor control example especially PMSM based on DSC/KV58/KV46..., because the KE0x is not used in PMSM sensorless control, so we have not the example for KE0x family.

BR

xiangjun rong

0 Kudos
Reply