GCT appconfig.h

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GCT appconfig.h

1,708 Views
fasihahmed
Contributor IV

How to change the DSC type from MC56F82748 to MC56F84763 without using Graphical Configuration Tool. 

I would like to change it using appconfig.h file. What are the steps for it?

Do i also need to add MC56F84763.h and MC56F84763.mem and MC56F84763 .tcl files from somewhere?

Labels (1)
0 Kudos
Reply
1 Reply

1,640 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Fasih,

I suggest you  use CodeWarrior for MCU platform to create a NEW project based on MC56F84763, then copy the source code from project based on MC56F82748, then compile, it is okay.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply