Download link: Suite56

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Download link: Suite56

11,607件の閲覧回数
vinzentmeier
Contributor I

Hello everyone,

 

i cannot find a download link for Suite56

Suite56 for DSP 566xx/DSP563xx|NXP 

 

How to get those files? Is the link still hidden somewhere?

ラベル(1)
0 件の賞賛
返信
12 返答(返信)

11,000件の閲覧回数
jameszaiter
Contributor I

Hi

The link you supplied is for DSP56300 family

I have the DSP56651 and require suite56.

Have you a link for this software as the downloads section says it is in archive

regards

James

0 件の賞賛
返信

11,000件の閲覧回数
jameszaiter
Contributor I

Hi Rong

i need the debugger/emulator

regards

James

0 件の賞賛
返信

11,000件の閲覧回数
jameszaiter
Contributor I

Hi Rong

also the programmer

0 件の賞賛
返信

11,000件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, James,

The asm56600.exe is the assembly compiler, dsplnk.exe is the linker, which are located at:

.......\dsp56600tool1.0\clas

The gds56600.exe is the debugger which is located at:

....................\tools\dsp56600tool1.0\ads

There is not programmer, if you want to program the application code to external flash, you have to develop the code yourself. this is the procedure:

1)write the application code and load it to internal RAM by debugger

2)write the boot code which can read the application code and write to external flash, then load the boot code by debugger and run.

3)use the bootstrap code in the on-chip ROM to read the application code from flash to RAm and run after power up automatically.

As I said the DSP566xx is very very old, we no longer support the tools.

BR

Xiangjun rong

0 件の賞賛
返信

11,000件の閲覧回数
jameszaiter
Contributor I

Thanks Rong

0 件の賞賛
返信

10,997件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I attach the tools for the DSP566xx, the tools has been obsolete for a long time, we no longer support it.

BR

xiangjun rong

0 件の賞賛
返信

10,997件の閲覧回数
jameszaiter
Contributor I

Hi Rong

i have this already but really need suite56 files.

Is there any way you can find a copy

regards

James

0 件の賞賛
返信

10,997件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, James,

Can you tell me which files you need? do you need the tools or tools user guide or reference manual of DSP566xx?

BR

Xiangjun Rong

0 件の賞賛
返信

10,997件の閲覧回数
vinzentmeier
Contributor I

This works. Thanks!

BR

Vinzent

0 件の賞賛
返信

10,996件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I attach the suite56 tools here, hope it can help you.

BR

Xiangjun Rong

9,268件の閲覧回数
preston29
Contributor I

或者您有没有Symphony Studio for dsp56000?

 

您是在摩托罗拉工作吗?

0 件の賞賛
返信

9,272件の閲覧回数
preston29
Contributor I

您好,感谢您提供的suite56 for dsp56300 和 GDS 56,我已经下载了,很好用。

请问您有没有suite56 for dsp56000? 能共享一下吗?多谢您了!

0 件の賞賛
返信