Debugger errors - Multilink FX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugger errors - Multilink FX

ソリューションへジャンプ
2,869件の閲覧回数
TurboMan
Contributor IV

I'm using a Multilink FX to connect to an MC56F8345.

I've verified the debugger is ok by connecting to a 56F84789, and also managed to connect to the 8345 previously.

Now when I try to connect to the target (56F8345) for a debug session, I get the following error:

Multilink_Error.jpg

I have tried the following:

* Multiple speeds (slowest, fastest, and others. Default is (24). )

* Creating a base example project for the 8345 using USB Tap and also separate project for Multilink FX

* Updating Multilink software

* Deleting the .metadata folder in the workspace and re-importing the CW10.6 project.

* Deleting the debug configuration and specifying a new one

None of the above has worked. I could connect into the target hardware last night, but have now lost that ability

Any suggestions welcome...

0 件の賞賛
返信
1 解決策
2,736件の閲覧回数
TurboMan
Contributor IV

False alarm...

Found a solder whisker shorting out a clock pin / pin near the clock input. Debugger working correctly now...

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,736件の閲覧回数
TurboMan
Contributor IV

False alarm...

Found a solder whisker shorting out a clock pin / pin near the clock input. Debugger working correctly now...

0 件の賞賛
返信