DSP56F807

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DSP56F807

2,135 Views
štěpánpodhorský
Contributor I

Good morning,

 

can somebody tell me if it is possible to check

somewhere on freescale website how long will

be produced DSP56F807 microcontroller?

 

Thank for all answers.

Štěpán Podhorský

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,881 Views
Martin35804
NXP Employee
NXP Employee

Hi.

For instance for DSP56F807VF80E check the product summary page that you can get from Buy section of the product page:

http://www.freescale.com/webapp/search.partparamdetail.framework?PART_NUMBER=DSP56F807VF80E&lang_cd=

In general information you will find following information:

Life Cycle Description (code)PRODUCT MATURITY/SATURATION
StatusActive
Application/Qualification Tier10-YEARS APPLICATION LIFE

When you click on life cycle you will see the description valid for the stages.

When you click at Application you will see the description valid for the 10 year application.

A PLC code does not mean that a part will be available for any specific amount of time. For example some parts have a PLC code of "4" for a few years; some have a PLC code of "4" for more than 20 years.  The life of a part is primarily determined by market demand.

When a product is not in the Product Longevity program Freescale cannot estimate the future availability of the part, which is primarily based on market demand. Freescale has no known plans to end of life the part.  When a decision is made to end of life a part, Freescale provides a period of time (generally one year) during which customers can place lifetime buy orders.

Product Longevity program link:

http://www.freescale.com/webapp/sps/site/overview.jsp?code=PRDCT_LONGEVITY_HM&fsrch=1&sr=1

For a full explanation of all statuses, take a look at the details of our Product Life Cycle (PLC) codes.

http://www.freescale.com/webapp/sps/site/eialink.jsp

I hope this will help.

0 Kudos
Reply